• RE: Regarding REF_MUX_CTRL[7:6] bitfield for Internal reference on EVAL-AD7779FMCZ(AD7779)

    Hi, 

    Apologies for missing this item. But to answer this query. You can use either of the two settings. The figure 98 you mentioned, is a suggested way to connect the internal reference to the external reference's input (but remember to configure the ADC…

  • Is the LT8316 compliant with energy efficiency level 6?

    Hi,

    I want to use LT8316.

    I'm considering it for an AC adapter,
    I am wondering if it is a product that can meet energy efficiency level 6.

    The rules are as follows,
    Is the LT8316 Level 6 compliant?

    www.cui.com/efficiency-standards

    Best Regards,

    Nao…

  • LTC1569-6

    I use LTC1569-6 with external clock. But periodically, I want to stop external clock and set at pin DIV/CLK "0" signal from microcontroller. Is it correct?
    As I understand, in this case the DC offset will increase. Will this DC offset be stable…

  • ADA4420-6

    I am looking for a video filter IC for VGA 1280x1024 @ 60 Hz signal, can i use ADA4420-6 IC for this application, please let me know

  • ADA6610-6 OUPUT

    I'm considering adoption of "ADA4410-6".
    How should I do the output terminal which isn't used?
    Is it OPEN? Is it terminated 75 Ω?
    If there are more good ways, please tell me.
    Please

  • AD9371 Questions 6

    Hello,

    I am testing the AD9371 Rx path using the ADRV9371-W/PCBZ EVB.

    I am using the Xilinx, HW-Z7-ZC706 Rev: B evaluation platform and the TES software to control the EVB.

    Rx Profile:  100MHz, IQRate=153.6MHz, Dec5
    The Rx PLL frequency is 3410MHz. The…

  • SPDIF ADAU1445/6

    hello

    I'm using ADAU1446, I want to use spdif sending 8 digital outputs through the optical fiber.

    And 'possible to use the spdif output of the DSP or do I have to use an external component?

     

     

    thanks

     

     

    Maurizio

  • AD9102 /6 - Any

    Dear Supporter

    Is there an example/script for the AD9106 or AD9102 setting the RAM as Tuning Word source?

    If it doesn't exist, please a provide a set of commands required to run several TW loaded in the RAM.

    This info is missing in the Wiki quick…

  • we have Virtex-6 FPGA ML605 Evaluation Kit.we want interface with AD9361 RF Transceivers.so  i want Know which board is suitable for our Virtex-6 FPGA ML605 Evaluation Kit


    hi,

               we have Virtex-6 FPGA ML605 Evaluation Kit.we want interface with AD9361 RF Transceivers.so  i want Know which board is suitable for our Virtex-6 FPGA ML605 Evaluation Kit