• Problem of AD7908.

    Hi ,

    I use the AD7908 and the current sensor IC "MAX4073T" without any OP between current sensor output and Vin of AD7908.

    In some case, the output of current sensor will be 0.4V, but there is a 3.6V rising due to the reverse current of ADC…

  • AD7908 Voltage problem

    Hello,

    I am using AD7908 in one of our designs. I am providing 5V at AVDD input ( Pin-5,6) and 3.3V at VDRIVE input (Pin-19). Please refer below picture. I have 24V-5V power supply and 5V-3.3V power supply on my board.

    When i turned off 3.3V power supply…

  • AD7908 full scale value

    Hello.

    For the conversion output of the AD7908, the value at full scale input fluctuates.
    The AD value changes according to the voltage of the previous channel.
    Measured at 5 V full scale.
    Condition 1 VIN 1 = 5 V, VIN 2 = 5 V AD value 255
    Condition 2 VIN…

  • RE: AD7908BRU –1V transients on the SCLK pin.

    Hi-

    I moved this question about the AD7908 to the Precision ADCs community.  Someone there should be able to help.

    Regards,

    AndyR

    EngineerZone Community Manager

  • RE: ad7928读写控制问题

    您好!

    不能正常读到数据请先检查硬件设计,看硬件设计是否正确,硬件设计请参考附件内AD7928评估板原理图。确保硬件设计正确后,请检查焊接是否正常,通常虚焊或短路会导致芯片状态不正常。

    对于软件部分的检查,首先应保证初始化流程与数据手册中流程要求一致。在数字读写时,则应保证读写时序遵守数据手册中时序图。

  • SPI question on BF526

    I'm trying to get the bf526 to talk to the AD7908 over SPI.  It looks like I need CPOL = 1 and CPHA = 0, but when I choose this setting my select line stops going low when I'm trying to do a write.  The 526 manual says that when CPHA = 0, the SPI…

  • RE: AD7357 how to check the DC Accuracy in worst case condition

    Hi Kevin,

    I have attached some list of ADC that were Automotive Qualified. Do you have specific paramater that you are looking for an ADC? like Throughput rate, no. of channels, or Resolution.

    You can also visit the Analog Devices website and filter…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…