Original Question: Can't find Comparator AD790 in ADIsimPE Library by ghussini
How can I simulate AD790 if it's not in the library and AD website does not have spice model?
Verified Answer: RE: Can't find Comparator AD790 in ADIsimPE Library…
Original Question: Can't find Comparator AD790 in ADIsimPE Library by ghussini
How can I simulate AD790 if it's not in the library and AD website does not have spice model?
Verified Answer: RE: Can't find Comparator AD790 in ADIsimPE Library…
I have read the AD790 datasheet.
It is a question about the operating range of the AD790.
The AD790 data sheet says "Dual? 15 V Supply Operation".
And the AD 790 data sheet says "ABSOLUTE MAXIMUM RATINGS Supply Voltage ± 18 V".
The AD790…
Hi jcasey,
Thank you for your interest on the AD790. We're currently checking the possibility of the AD790 for supporting +3.3V logic and if we would be able to release a new grade or new product that could handle this condition. May we ask what specific…
Hi William,
You could look into AD790 particularly Figure 11 as well to implement a sine to square wave using a 5V single supply only.