• AD7880E Accuracy

    Hi I'm looking at the datasheet.

    I wonder why the accuracy specs(eg,Total Active Energy ) is defined as typical.

    Do you have min/max data?

    If not, how much percentage of vibration should be considered?

    Best,

    Tarzan

  • RE: Confirm whether we can use AD574ASD/883B in the design

    FormerMember
    FormerMember

    People want faster, more bits, and smaller packages, so more and more ADCs are serial.  However,

    you could look at the AD676, AD1674, or AD7880.   If you want an AD574, you will have to buy

    the 5962xxxx full mil part.

    Harry

  • ADE7880 constant values in AIRMS BIRMS CIRMS

    Hi,

    As part of preliminary phase for a smart meter board i am putting together a quick setup for SPI communication, i used an Atmega32u4 AVR directly connected to the ADUM1401 of a commercial samrt meter we used in the system previously, i also connected…

  • RE: ADE7880 Calibration Set up

    Hello Gary and thanks a lot for your answer. There is something last that i would like to be defined:
    In the application note regarding the calibration of the ADE7880, is a unit called calibration inputs. For each calibration step the voltage and the current…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…