• AD7847

    Timing about AD7847:

    In the AD7847 datasheet, I got the truth table and write timing diagram as below:

      

    I have confusions:

    (1) from the truth table, I think that both CS and WR rising edge can latch data into the DAC.

    (2) But from the timing diagram…

  • AD7837/AD7847 DAC interface

    Dear All,

    Can i make interface with DAC ( AD7837) using Microprocessor have I/O ports with logic voltage levels equal to 3.3 volt??

    and if not there is DAC with logic level I/O equal to 3.3 volt??

    Thanks in Advances,

  • RE: SiGe "BiCMOS" process devices

    Sure, I would like to know which of the following devices are SiGe based:

    • AD1674
    • AD2S80
    • AD676
    • AD7245
    • AD7712
    • AD7821
    • AD7847
    • AD7884
    • AD7893
    • AD7896
    • AD976
    • ADG526A
  • AD5544: Long term drift over time

    I need Long Term Stability parameter for the following DAC's :
    AD5544
    AD7847
    AD7846

     

    The long term drift over time is included in the max and min specifications of
    the part. For example, we guarantee that the full-scale gain error of the…

  • AD7847,0代码附近出现20mv的失真

    1.电源电压正负12V

    2.输入为有效值位7V的AC.

    3.设置为1111 1111 1111 时 输出正常,误差4个MV左右

    4.设置为0000 0000 0000 时 输出正常,误差4个MV左右

    5.设置1000 000 000时,理论输出0V,实际输出20mv左右(四个通道出现相同情况)

    5.设置1000 000 0001、1000 0000 0010、1000 000 0011,1000 000 0100时,实际输出20mv左右(四个通道出现相同情况),出现0v输出周围失真…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…