• AD7819: LSB is on DB0

    Which one is the LSB? DB0 or DB7? This is not clearly mentioned in the
    datasheet of AD7819.

     

    DB0 is the LSB
  • AD7819 use without micro processor

    I am wondering if anyone has any ideas on how to configure the AD7819 (or another similar part) to do continuous conversions without a controller like and FPGA or micro?  What I need to do is continuously monitor aDC voltage and have the ADC "free-run…

  • AD7819 Spice model?

    Is there a spice or IBIS model for this part by any chance? 

  • AD7819 missing datasheet information.

    I have to run the AD7819 with VDD 5 V and interface to 3.3 V tolerant inputs at the digital side. Max logic output voltage is not specified in the data sheet. The DB7..0 is specified to be TTL

    compatible and the BUSY signal is not specified at all. What…

  • AD7819的BUSY沒發送

    關於busy沒發送是偶發性的,也有確認timing也按照規格書的傳送。

    想問一下發生這個原因會有哪些可能性呢? 以及這有沒有什麼方法可以解決呢?

  • AD7819 in free run mode without processor

    Hi friends

    do you have ideas about using a AD7819 without a processor to drive it?

    thanks

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…