• AD780S:  Do you have any radiation reports, TID or SEE  for AD780S ?

    I am currently evaluating AD780 voltage reference. Since this product is QMLR,
    could you give me radiation reports (TID and SEE)?


     

    We have a TID radiation test report for the AD780S devices. See attached.

    Unfortunately, we do not have an SEE…

  • AD780 long term drift

    I have questions about the AD780 long term drift spec need your help.
    In the datasheet, the long term stability is +/-20ppm/1000hr (typical), and
    there is note for it, says "The long-term stability specification is no
    cumulative. The drift…

  • RE: AD780 with 2,56V Vout

    Hi,

    I moved the thread to Voltage Reference as part of the objective to close all open threads in the Amplifier community.
    The thread might be old but may be useful to other users that might have the same concern.

    Thanks!

  • AD977A: is it possible to use one AD780 to be the ref voltage of 16 AD977A for +-10V range?

    Is it possible to use one AD780 to be the ref voltage of 16 AD977A for +-10V
    range?

     

    It will cause problems. For AD977A, there is a current from AD780 to R3IN (See
    circuit in fig 16a/16b, attached).  Therefore AD977A will interfere others. You…

  • AD7980 Ref Input Driven by AD780

    Hi Team,

    I am planning to use AD7980 with AD780. Do I need to use a buffer between AD7980's ref input and AD780's output? From the datasheet of AD780, it looks like it already has a built-in buffer.

    Thanks.

  • AD780 +Vin Pin and DNC Pin Problem

    Hi All,

    End user raised up the below question for un-powered I-V curve tracing with input voltage between both -5V to 5V and -1.5 V to 1.5V. No application or on-board test result available. 

    According to the un-powered curve tracing, pin 2 (Vin-power…

  • RE: AD780 Noise ?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD780 EOL or LTB?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • could we have the Quality report for the Die AD780-001C

    ould we have the Quality report for the Die AD780-001C