• AD7799: SPI issue

    My customer has problems with the SPI interface of the AD7799.  When he wants
    to read out e.g. the status register, he gets as a response two bytes with the
    value "0". The schematic was checked two times, so we are quite sure that there …

  • AD7799: Changing channels

    Works 100% in a single channel application. Am trying to switch channels on the
    fly. Will allow me to change channels on initialisation but not during run
    time?

     

    When the channel is changed with this family of products, the ADC is
    automatically…

  • AD7799 convert error / AD7799转换出错

    使用AD7799,有时候会很偶尔地出现转换时间过长,并且转换数据出错的问题,但是掉电重启后又恢复正常,请问有可能是什么原因造成的?大家有遇见过类似的问题吗?

    when I use ad7799, sometimes the conversion time is too long and the conversion data is wrong, but it returns to normal after a power failure. What could be the cause? Has…

  • AD7799 AVDD Monitor 1.17V Internal Reference

    When monitoring a voltage on the AVDD pin, what is the accuracy/stability of
    the 1.17V internal reference used for analog-digital conversion?

     

    For the AVDD monitor, an internal untrimmed 1.17V reference is used. AVDD is
    divided by 6 and the…

  • AD7799: Problems with communications via serial interface

    I use AD7799 in recommended circuit in continuous conversion mode on 1 channel
    (1st). Sometimes (perhaps due to EMI) I have some problems with serial
    interface. recommended way of reset (32 '1') works, but I can't determine the
    moment…

  • I have a question about the timing of AD7799.

    I have a question about the timing of AD7799.
    The Datasheet  says "Ready Bit. Cleared when data is written to the data
    register. Set after the data register is read or after a period
    of time before the data register is updated with a new conversion…

  • RE: AD7799 Conversion

    Hi, 

    Looks like this question was just transferred from a different community and might be long overdue. However, for others who may find this a similar issue let me try to address this. 

    First, yes you are correct the absolute AIN voltage limits (unbuffered…

  • AD7799 内部放大器是什么放大电路?

    AD7799 有一个可编程的内部放大器。他是一个什么功能的放大电路,是同向?反向?差分? 还是其他功能的,望解答。谢谢!

  • RE: I would like to receive the RoHS certificate of AD7799

    Hi,

    Apologies. I know this is long overdue. But just in case you still need some help or if someone have similar concern.

    The 'Z' suffix in the ordering guide means that this model is RoHS Compliant. See the general compliance document, here.