If REFIN is tied to VDD on the AD7787, is the AIN2 input voltage range from GND to VDD (when configured as a unipolar input)? Are there any issues with that configuration? VDD=5V in my application.
If REFIN is tied to VDD on the AD7787, is the AIN2 input voltage range from GND to VDD (when configured as a unipolar input)? Are there any issues with that configuration? VDD=5V in my application.
Hi,
I am wanting to use the AD7787 for reading two single-ended signals, but one of the inputs is a differential input. I am guessing I can tie the - signal to ground and simply drive the + input with my single-ended voltage. i am hoping that by doing…
Hi people!
I just bought an ad7787 and I cant get it running.I have read the code you attached but Im having some troubles understanding it, probably because my knowledge about C is not that good. Anyway, I have connected the device to a atmega1281 that…
Hi people,
I have just bought an AD7787 and am looking to interface it to a Microcontroller. Does anyone have any example code for getting the device up and running.
I have had a look at the datasheet and there isn't a section with some example code…
AD7787的2个通道分别是差分输入和单端输入,那如果要用AD7787实现2个单端输入如何实现?或则有没有别的型号代替,精度要求24位。
AD7787的2个通道分别是差分输入和单端输入,那如果要用AD7787实现2个单端输入如何实现?或则有没有别的型号代替,精度要求24位。
Hi Jovialjha,
Below is the short list of Sigma delta ADC that possibly fit to your requirement.
ADI Sigma-Delta ADC portfolio range from 8bit to 24 bit resolution. And these parts are available with their evaluation board and software, you can visit…