• AD7782滤波电路

    热采用2.5V电压基准,使用内部放大测量0-120mV信号,应该怎么选择RC滤波的值呢?实际测试时会有出现测量结果一直下降的现象,是否滤波电路引起的?

  • Master/Slave SPI selection on AD7782

    For the AD7782, how do you set the MODE pin to achieve MASTER and SLAVE?

    The current version of the datasheet posted on the web site (http://www.analog.com/en/analog-to-digital-converters/ad-converters/ad7782/products/product.html, version 2001 rev0…

  • RE: AD623测量热电偶时的一些问题

    R21 0R未连接?

    AD623哪里买的?

    电路可以先用Multism/LTSpice仿真一下。

    另外,3位数字的老料,我们一般不推荐再继续使用了。

    http://www.analog.com/cn/ad623

    建议评估下AD8226/AD8221,或者超便宜的固定增益的AD8293G80/160,或者索性一步到位,用热电偶场合专用ADC, AD7124-4/8, 不需编程配置的AD7782之类。

  • AD测量0-5V电压信号

    如题,使用AD7782测量传感器输出的0-5V电压,应该如何搭建硬件电路呢?有几个问题请教大家,

    1:根据手册,测量端Absolute AIN Voltage Limits范围是(GND+100MV,VDD-100MV),是不是意味着输入的两个引脚都必须是相对与AD的地有100mV的偏差呢,比如被测引脚A应该是0.1V-4.9V,被测引脚B也是,但是实际中被测引脚A就是地,被测引脚B会有0-5V变化,应用时是需要将被测信号抬升100mV吗?

    2:由于后端接3.3V单片机MSP430,5V的AD和3…

  • Sigma -Delta ADC常见问题解答

    ADI 拥有一系列种类齐全的高分辨率低带宽的Sigma-Delta ADC 产品,这些产品不仅集成了ADC,还集成了电流源、多路开关、可编程增益放大器PGA,模拟输入缓冲等等。

    附件中是 Sigma -Delta ADC常见问题解答 ,欢迎小伙伴们下载~~

  • RE: ADuC845 Calibration Logic

    Chopping on delta sigma delta ADCs is a technique that can be used to cancel offset voltages and other low frequency errors. You can read more about it on the attached file.

    For the ADC conditions during calibration, it is recommended to use the slowest…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…