• AD7770-Query

    Hi ,

    1.Is this IC AD7770 SIL certified ? Can this be used for a design that is to be SIL certified ?

    2. Also can we sense 0-200 mA using an external sense resistor through this IC. If so, what will be the sense resistor to be connected? In datasheet it…

  • AD7770 ADC Error

    Hi,

    Kindly share the INL Error, Gain drift error and PSRR of AD7770 for analog input and voltage input

    Also What will be the adc error while using internal and external reference.? 

    Warm regards,

    Monisha OM

  • AD7770 PIN Tolerance

    Hi ,

    I am using AD7770 For high side sensing(24V). Is the analog pin is 24V tolerant ? Or else we need to use voltage divider which will effect on accuracy.

    Kindly reply me.

  • RE: AD7770 Data output interface

    Hello,

    How are you using the SYNC signal so? The AD7770 is a sigma delta ADC so it will continuously run conversion managed by MCLK. SYNC_IN is just a synchronization input, that you may eventually issue if your DRDY is out out sync of a given synchronization…

  • AD7770

    Hello!

         I have question regarding the analog channels of the AD7770: are the analog channels isolated in AD7770? Can they be coupled directly with signals coming from plcs? Isolation amplifiers required for AD7770 if necessary?

    Thank you!

  • AD7770 questions.

    Hi.

    I have two questions about ad7770.

       1. how long time to start and finish the conversion?

           'sar' has timing data(conversion time) on the data sheet, but no 'delta-sigma'.

       2. When does 'MCLK Switch Error' occur?

          I am trying…

  • AD7770 Temperature Sensor

    I’m using an AD7770 as my main ADC on a custom board I’m designing. I’ve been playing with some prototypes and experimenting with the AD7770’s built-in temperature sensor. Using the code from ADI’s website I’m reading back some odd values for temperature…

  • AD7770 maximum range

    Hello,

    I'm using the Eval Board of AD7770.

    The maximum amplitude I can measure between AIx+ and AIx- is +/- 1.65V (dual supply operation)

    According to the AD7770 datasheet, he noted that the maximum amplitude is +/- 2.5V (according to table 11 of…

  • AD7779 and AD7770

    Hello,

    I have a question about a differencis of digital flter between AD7770 and AD7779.
    Attached file is the rms noise and resolution performance table from the datasheet.
    AD7779 and AD7770 have same combination of ODR and Decimation Rate excluding 32kSPS…