Hi Manan
you would need a driver to connect the electrodes to AD7768 and the high impedance electrodes cannot be wired directly in to AD7768
Hi Manan
you would need a driver to connect the electrodes to AD7768 and the high impedance electrodes cannot be wired directly in to AD7768
Any SPI timing waveform which follows the AD7768-1 SPI timing in the datasheet will be fine. You may make your raspberry4B interface to be compatible to the datasheet timing.
Hello,
We are using AD7768 for one of our application. We require following things to fix our design.
1) What is the full scale input power level of the ADC in dBm , this detail is not provided in the ADC datasheet. Reference voltage to ADC we are providing…
Hi,
As you know, enable the CNV pin on the SAR ADC, it can control when it begin to capture signal accurately. But for AD7768 or other sigma detal ADC, Can it do this? If yes, how to do it?
Thanks!
最近在用FPGA控制AD7768进行数据采集,用的pin模式,感觉控制管脚都接对了,输出的dclk和drdy也是对的,但是输出dout7-0不对,有用过AD7768的吗,可以留个联系方式或者回复我一下,如果问题解决了,可以给发个大红包,真是着急!!!!!!!!!!!!
Recovered the answer below.
Hi John,
If you are using a single DOUT then you should also use pin 21 (DOUT6) on the AD7768.
Regards.
Hi,
I would like to check in and see if I am NOT planning on daisy-chaining or using the synchronization feature of the AD7768, what shall I need to do with the nSYNC_IN, nSYNC_OUT, and nSTART pins? Is there going to be any problem if they are just held…
Reference P50, rev B of the AD7768/AD7768-4 data sheet.
This states that SCLK idles low and this is illustrated in figure 80 on P51.
Why then does figure 79 on P51 show SCLK toggling while CS is high ?
Hi,
I would like to use the AD7768 in 4+4 chan interleaved mode do acheive near to 512ksps. Is it possible to use the CLK_MOD_DEL_EN setting to achieve this? What does this register do, its not described in the datasheet.
Thank you.
Dear members,
we use the AD7768
batchcode #1626 gets 5°C warmer than batchcode #1527 and consumes more power
What is the difference?
(same Code same PCB)
best regards
Rainer