FAQ
Hello,
I have planned to use the AD7741 to perform Voltage to Frequency conversion.
My configuration is :
- External reference 2.5V +/- 0.1%
- External clock from a quartz of 32768 Hz
With the configuration described above the AD7741 response…
Hello,
I have planned to use the AD7741 to perform Voltage to Frequency conversion.
My configuration is :
- External reference 2.5V +/- 0.1%
- External clock from a quartz of 32768 Hz
With the configuration described above the AD7741 response…
I'm attempting to measure the true 'average' value of a time varying signal over a variable time interval. The input signal varies between 0 and 2.5 volts but may have components from near DC to a fixed frequency of a few hertz. The time interval…
Dear Sir/Madam,
I am just studiung about your V-F converter AD7741.
Do you have a good solution over 3MHz output to use your AD7741 or another V-F converter?
On your datasheet AD7741 can output 2.7648MHz.
(This come from max. output freq=0.45x fCLKIN…
Hi, may I extend this discussion about AD8495?
I try to use AD8495 to measure K type TC from 15 to 1100 deg.C.
The output of AD8495 is about 5.5V at 1100 deg.C.
I will supply 6V to +Vs pin of AD8495.
But for isolation consideration, I plan to connect…
Team,
I have a customer that is ready to start a prototype for their next generation air quality measurement instrument.
They are asking whether or not the AD7741 is a smart option for this project, or if there is a better V-F converter ADI can offer…