• RE: AD7734 Init() failure from the generic drivers provided AD7734.

    Which carrier/ board are you using?

    We have some examples for some hosts/carriers like Zynq, RPi, Arduino.

    I took a look at the AD7734 generic code, and that one doesn't seem to implement SPI. Which means it should be carrier/host specific.

  • Using AD7734 board with LabView ?

    Hello,

    I am new to Analog Device boards,

    We have AD7734 evaluation board and I was wondering if i can use it with LabView ?

    If not, how can use this board with iMac ?

    Thank you

  • Calibration procedure for AD7734

    Hi,

    I have AD7734 Evaluation board.I connected external microcontroller.Iam able to read the sensor digital output.The sensor analog output  value with a multimeter and the sensor output after the ADC conversion values are not getting same.I feel the ADC…

  • Eval AD7734 Init() failure

    Hi,Im a new bee to coding, I have EVAL-AD7734 board with me.I downliaded genericdrivers AD7734.h and AD7734.C files.When I try to understand the Init() function, it always go to the unsuccessfull status 0X00.Please anyone make me understand.I even got…

  • AD7734 sampling rate

    Hi,

    I'm using an AD7734 ADC to take sensor readings but the sampling rates I'm getting from it seem to be slower than indicated on the datasheet for a given filter word. Shown in the table are the specced conversion times and the conversion times I have…

  • RE: Communication Problems with AD7734

    This question has been closed by the EZ team and is assumed answered.
  • RE: Single conversion mode in AD7734

    This question has been closed by the EZ team and is assumed answered.
  • EVAL AD7734 not able to access through my PC

    Hi,

    I connected +5v and ground of external power supply to DVDD and DGND of the Evaluation kit respectively.I opened Easy start application then I selected the com port 1 and when i tried to follow next instruction to reset the board ,I got an error showing…

  • AD7734烧芯片

    AD7734,莫名其妙就烧了,很严重的那种,发生过几次了,请问,会是什么原因呢?谢谢

  • ADC AD7734 CROSS TALK

    Hello 

    I am using all the 4 channel of AD7734  ADC .

    When I vary any  channel input voltage  it gets reflected in the other channel.

    Following are the configuration value of the ADC 

    REG (28H - 2BH) : 0AH           //CH Enabled and ADC range  -5 to 5 Volt

    REG (30H…