• AD7725: FSK modulator

    Do you have a solution for a simple FSK modulator/demodulateur (f1 25 Hz and
    f2"25 Hz at 300 bauds) using AD7725 ?

     

    The AD7725 cannot be used to directly demodulate. It samples the input and
    provides a programmable digital filter…
  • AD7725  ADC - OBSERVED DISTORTION IN BIPOLAR CONFIGURATION

    Hi,

                 We are using the  ADC AD7725 in our design.In that we have tested the ADC in Unipolar mode and the output  looks good with very low distortion.  We are facing problem in testing of  Bipolar configuration. Our Analog Input Range is  -2V to +2V Single…

  • Problem in AD7725 operation at input Frequency between 9.12MHz to 9.3MHz-Need Immediate Support

    Hi,

           We are using AD7725 with Bipolar configuration and loaded Default Filter configuration .We are feeding the External clock for its operation from 5MHz to 10MHz to its clkin pin.we have tied XTALOFF to high and disabled the XTAL functionality.

        In…

  • RE: ADC used for single-pulse conversion

    Hi Postino,

    Here are some list of ADC that could be suitable for your application. You may also wanted to check the ADI website and do a parametric search and put in parameters on the ADC that you wanted to search. Please refer to the link below.