I would like to use sigma-delta converters for a multi-channel (48) acquisition application. There is a stringent need for synchronicity between each converter in our application.
I am interested in using AD7712 converters since it features…
If he wants to input +/-10V single-ended signal to AIN2. What power supply should he use? Single 5V, single 10V or +/-5V? I can not find very clear statement in the datasheet.
A
For an analog input of +/-10V on the channel, a supply of +/-5V can…
In AD7712 data sheet, pages 11 and 12, noise is specified as total rms value. I would like to know noise spectral density ( in particular for a 1kHz notch frequency selection and in a 1 mHz to 1 Hz bandwidth ). Have you got some specifications or…
In our application, some AD7712 use System Offset Calibration initiated, after the power-up, together with the device configuration, by the means of a single writing of the Configuration Register (0x8297A1). In our case, the calibration duration…
This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.
This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.