• AD7708 big defference offset value between system and internal calibration.

    Hello,

    When do zero calibration result compare between system and internal calibration, there is a big difference.

    After Internal calibrattion, offset register value nothing to change from 0x8000.

    But when do system calibration with AIN 0V, offset…

  • AD7708轉換無法達到滿刻度(0xFFFF)問題何解??

    我在使用AD7708進行ADC轉換時發生無法轉換到滿刻度現象,狀況說明如下:

    1. 採用偽差分模式
    2. REFIN1+ +2.5V ; REFIN1- GND
    3. AICON +2.5V
    4. AIN1 接類比輸入電壓範圍(2.5V~5.6V)
    5. AD7708暫存器 CHOP = 0; NEGBUF
      = 1; REFSEL = 0; CHCON = 0l OSCPD = 0;

    當我將AIN1電壓輸入調整至5.6, 應該可以觀察到REWDATA = 0XFFFF 但是無法達到滿刻度…

  • AD7708启动卡在零点校准,不能正常启动。

    使用AD7708的产品在做出厂频繁上下电测试时,发现AD7708会在零点校准时,查询mode寄存器里面的MD2~MD0,一直都不是001 idle mode。

    1. 程序是这样写的,每次上电后都会对每个通道进行零点和满度校准。

    2. 上下电情况:上电后,等待大约几秒钟MCU刚正常工作,下电,然后立即上电。断电的时间极短,在百ms左右。

    3. AD7708的复位是直接接到5V的。

    请问这种情况,是由于断电时间过短,再上电,AD7708没有完全复位造成的吗。谢谢

    之前做过其他工况的上下电实验(上电,下电都保持30s以上…

  • AD7708 转换结果时而正常,有时候变得特别慢

    有两台样机使用AD7708,相同程序,一台正常。另一台AD转换速度有时候正常,有时候特别满。用示波器查看ready引脚信号,也能发现输出波形也很慢。

    重新焊接了,也没啥问题。请问这种情况应该怎么排查问题。谢谢。

  • AD7708偶尔上电死机或者可以说SPI无响应

    设计信号采集板,发现在外部端子连线较多情况下,重新上电出现死机现象,但不是每次。reset引脚我一直接VCC.难道上电还需要reset吗?

  • RE: 请推荐几款A/D芯片

    AD7708,AD7949,AD7124-4等。

  • Here we are attaching the bridge circuit as shown in figure:1 and the ratiometric measurement system using AD 7708 as shown in figure:2.We have checked the hardware for the ratiometric measurement as shown in the figure:2 schematic and separately for...

    We have captured the digital data from the ADC (AD7708) for 1V and got the corresponding results. When we gave bridge output to instrumentation amplifier and then amplifier output to ADC, got output corresponding to 1V and when we connect bridge output…

  • AD7190_AINCOM范围

    下面是AD7708的AINCOM范围限值。但对于AD7190,我找不到关于AINCOM范围的类似参数。能否请您提供此数据?

  • RE: 5V voltage reference for the AD7718?

    你好,今天看到了这个帖子,AD7708/ad7718如果要测量0至5V的输入电压范围,只能在伪差分模式下工作吗?在全差分模式下,可以吗?比如,AIN1/AIN2,将AIN2接上2.5V?

    谢谢,期待你的回答