使用AD7708时发现,偶尔设备重新上电,CPU采集到AD7708输出的码值为全0或都32767.不知道是怎么回事,大部份时间芯片能正常工作,就是上电的时候会出现所有通道采集到的值都不变,一直是0或32767.以下是硬件和程序。断电后重新启动故障消失,芯片工作正常。
这是硬件连接,基准电压是2.5V,单端方式工作。
INT8U channel2[10] = {0x0f,0x1f,0x2f,0x3f,0x4f,0x5f,0x6f,0x7f,0xef,0xff}; //0-10v==0-65…
使用AD7708时发现,偶尔设备重新上电,CPU采集到AD7708输出的码值为全0或都32767.不知道是怎么回事,大部份时间芯片能正常工作,就是上电的时候会出现所有通道采集到的值都不变,一直是0或32767.以下是硬件和程序。断电后重新启动故障消失,芯片工作正常。
这是硬件连接,基准电压是2.5V,单端方式工作。
INT8U channel2[10] = {0x0f,0x1f,0x2f,0x3f,0x4f,0x5f,0x6f,0x7f,0xef,0xff}; //0-10v==0-65…
Hello All,
Does anyone know if AD7708 can interface with Arduino using the SPI interface? Looking through the datasheet, other microprocessors are mentioned but the not the Arduino. Thank you!
Dear Analog Devices,
Is the Linduino programming library compatible with the AD7708 ADC?
Thanks,
toshiyo
Hello, Sir:
Have any AD7708 sample code or initial code availabe on Website?
Hello there,
I have a question about the absolute ratings of the AD7708.
According to the datasheet:
AVDD to DVDD . . . . . . . . . . . . . . . . . . . . . . . . –5 V to +5 V
Typically, in my design: the AVDD is a 5.7V and DVDD at 3.3V; within the…
Hello,
in our applications we are using 6pf and 12 pf watch crystals
We don't recognize requirements for AD7708 oscillator. Have we to use a 6pf crystal, a 12pF one or we can use both without problems?
Thank you for your help
Andrea Gonelli
大家好,想请教一下大家在使用AD7708采集0-2.5V电压时,有遇到过采集的码值非线性情况吗,最近使用AD7708时,发现AD7708采集的码值是非线性的,用示波器看了模拟量回路的绞波VPP=85MV.请大家帮忙分析一下,是怎么回事以及怎样补偿?以下是测试数据。
输入电流 | 采集码值 | 递增值 |
0mA | 18 | |
1mA | 1512 | 1494 |
Hello there,
With the AD7708, we are experiencing a strange behavior with sudden changes of temperature.
If there is a rapid cooling of the device down to -40 Celsius, it happens that a reading is completely erroneous.
This behavior happened when…