• I do not receive data from AD7707

    I used to work with AD7705. Now I need to configure 10 boards with AD770test AD7707.RAR7. I am getting wrong data from the chip. What am I doing wrong?

  • AD7707:input impedance and currents

    I´ve got some questions about the specifications of the AD7707. I´m working
    actually with the low level inputs. I didn´t found clearly values about the
    input impedance or input currents in buffered or unbuffered mode in the data

  • AD7707 update version

    could you please advise ADI AD7707 replacement parts ?

    customer need to upgrade them product, we need similar parameter such as range, gain and input mode. 

    many thanks .

  • RE: AD7707 and reference voltage

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD7707要停产了吗

    AD7707要停产了吗?现在市场卖家说这款产品封装要停产了,改其他封装,请问下有没有哪款产品可以代替,谢谢!

  • AD7707的采样速度问题

    我使用AD7707设计产品,晶振4.9152M,使用模拟开关8通道切换,每通道工作在50HZ,但是每各通道的增益不同,目前已经能读到数据,但是在速度方面不高,115200的时候只能4次/秒,但是按照计算115200BPS,按照每次发送8个字节指令读取,返回7个数据指令,应该可以做到10次/秒,我不是很清楚问题出在哪,我如果设置采集速度为250次/秒,也只能到5次左右,另外我没有找的AD7707哪地方有个CODE寄存器,附件是读写和设置程序,请帮我看下是什么问题,以下是设置程序:

    void AD_AINT3…

  • AD7790: Shift signals

    Sensor output is amplified so that signal lies between -3 and +3 V. System
    voltage is 3 V, -3V available from a voltage converter.
    Is it possible in some way to use the AD7790 as ADC in that case? What other
    possibilities are there to convert…

  • AD7712: Master clock

    I would like to use sigma-delta converters for a
    multi-channel (48) acquisition application. There
    is a stringent need for synchronicity between
    each converter in our application.

    I am interested in using AD7712 converters since
    it features…

  • AD770x经典仪表转换器常见问题解答

    AD7705和AD7706均为完整16位、低成本、Σ-Δ型ADC,适合直流和低频交流测量应用。其具有低功耗(3 V时最大值为1 mW)特性,因而可用于环路供电、电池供电或本地供电的应用中。片内可编程增益放大器提供从1至128的增益设置,无需使用外部信号调理硬件便可接受低电平和高电平模拟输入。

    AD7705拥有两个差分通道,而AD7706则拥有一个差分通道和两个伪差分通道。在定制比率应用器件时,差分基准电压输入还能提供极大的灵活性。

    AD7707是一款适合低频测量应用的完整模拟前端。这款3通道器件既可以直接从传感器接受低电平输入信号…