Q
What is the meaning of the absolute input voltage
A
The AD7864 is a replacement for the TI part ADS8321 so the product line has put
the “Absolute Input Voltage” spec in the general specifications section of the
datasheet (as in the…
Hi collegues.
I need ADC with really differential input and single supply.
-IN connected to reference point (REF/2)
+IN connected to input signal (+\- 2.5v)
I tried AD7684 but DataSheet tells that +IN and -IN MUST be in opposite phase to reference…
Hi Janmay,
Apologies for my delayed response.
I am assuming that you are using the AD7684-1. From your schematic with VinxB connected to AGND,the AD7684-1 is configure to have a +/-10V Range input voltage range.
1. On your first question that you are…
I managed to get some support on this issue. Sorry for the delay.
It turns out that the two interfaces will not match. They are quite similar, but the difference in MSB position, the duty cycle of the clock, and the number of clock cycles per sample…
Presenter: Michael Arkin
A typical signal chain starts with a sensor followed by an interface amplifier, signal conditioning blocks, an ADC Driver, an ADC, and a digital processing engine. Most digital systems have processing power to replace some…
Hi Jebas,
PLease see attached list of the ADIs some of the latest differential ADCs with less tahn 2 LSB INL error. I have short listed this ADCs for DAQ systems application. I have included in the column on the file the throughput rate and full power…
你知道心源性猝死(SCD)吗?
心源性猝死是指急性症状发作后1小时内发生的以意识突然丧失为特征的由心脏原因引起的自然死亡,而且心源性猝死90%以上发生在医院外,但是这类猝死病人的黄金急救时间只有5-10分钟,超过10分钟的抢救存活率不到1%。
当发生心源性猝死(SCD)时,唯一的救治手段是胸外按压+心脏除颤,及时除颤是迄今公认制止心脏猝死的最有效方法。
对此,ADI推出了自动体外除颤器(AED)解决方案,可以自动诊断可能危及患者生命的心室纤维性颤动和心室性心博过速两种心律失常症状。
自动一词提示器件可以自主分析患者状况…
AD9288 输入与输出的对应关系是什么??
http://ezchina.analog.com/message/9029#9029
AD5934模拟IIC通讯的问题
http://ezchina.analog.com/message/9724#9724
关于AD7763内部增益寄存器问题
http://ezchina.analog.com/message/9439#9439
AD7606采样问题