• RE: AD768S Accuracy

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD768与FPGA的连接

    AD768的数字输入的高电平最低电压是3.5V。
    而现在的控制器包括FPGA都是3.3V电平的。直接连接应该是会出问题的。

    1、那么有什么芯片可以将两者连接起来吗?ADI有什么推荐吗?

    2、AD768的时钟最高可达40M。那么有什么可用的时钟芯片吗?当然了,芯片也需要3.3V控制,输出时钟高电平为5V

    麻烦帮忙解答一下,谢谢

  • AD768输出无变换

             最近在使用ADI生产的DAC芯片ad768,根据其数据手册中的基本连接搭建的电路,如下图。

    使用按键模拟时钟输入。使用使用排针和杜邦线选择数字输入DB0~DB15的高低电平。

    发现无论输入什么值,IOUTA电压时钟为0,而IOUTB电压则为0.7v,不发生变化。一连几块试验板都是类似情况。

    请问除了是芯片本身损坏以外,还有什么其他原因。

                                                                     

  • 将AD768电流放大后的电压输出无变化

    我按照数据手册中的下图连接方式将AD768的输出电流转换成电压值。

    放大器用的是AD811,Rfb用的是120R。时钟信号的输入是晶振产生的27M的正弦波。

    其他的连接全部是按数据手册中来的。参考电压用的是内部2.5V参考电压,参考电压的输出是正确的。

    16个数据位的输入无论是固定在0还是65535,还是别的其他值,放大器的输出都是-2.4V左右,不会有改变。

    问:可能是哪些原因造成的这种错误呢?是晶振?还是对AD768的操作有错误?

    请帮忙解答一下,谢谢

  • AD768和AD9764的输出电流转电压的疑问

    这两款芯片都可以输出差分电流。我现在想转换成线性的电压输出。

    在AD768的芯片手册中有这么个图:

    手册中说,这样连接,放大器输出的电压在0~2V之间。但为什么我觉得是在-2~0V之间呢?IOUTA的电流范围是0~20mA,IOUTA引脚输出的电流不应该是流出DA芯片,流向放大器吗?这样算出的应该是-2V~0V吧

    下面的图24中,电流是流入DA芯片的。我想确认一下,按图23那样连,输出的电压信号会是0~2V还是-2~0V

    在AD9764的芯片中也有类似的问题。这样输出的电压值应该也是负值吧…

  • RE: AD768数据转换毛刺问题

    请问一下,你们在使用AD768的时候,数据位是使用74alvc164245的,那么时钟呢?是使用FPGA的普通IO口作为时钟输出然后接的74alvc164245吗?还是用的FPGA内部的时钟呢?还是其他别的方式提供的5V时钟呢?求教

  • AD768这款芯片为什么在新设计中不推荐使用?

    我没有找到比它更合适的芯片了。

  • RE: AD768 IBIS model

    There is no IBIS model for the AD768.

  • AD768电源问题

    最近在使用AD768芯片做DA转换,对芯片的数模部分处理存在一些疑问:

    1.AD768是采用双极性供电的,板子上有数字电源和模拟电源,那么AD768的电源应该怎么处理?现在做的是用+5v的数字电源和-5v的模拟电源,这样可行吗?

    2.由于存在上述的疑问,因此DA芯片现在的供电是不能保证完全对称的,这样对芯片有一些什么影响?

  • AD768 noise

    I am looking at the AD768 for the simultaneous generation of 64 high purity carriers between 1-10 MHz for a space application. The AD768 is old but that is the only space-rated >25 MHz 16-bit DAC with low noise that I have identified.


    Can anybody…