• AD7678: Driver

    data sheet for AD7678 says that its input driver must settle fast and be short
    circuit limited if its using different rails to the single rail ADC.
    It recommends the AD8021 for its performance. - But its by no means short
    circuit protected!
    -…

  • AD7678 ADC is not giving any value below 200mV

    I am using 3 AD7678s in a daisy chain for a precise test system. I have some problems with the outputs of AD7678. First problem is; I cannot read any values below nearly 200mV. I get hex'00000' output or hex'20847' output below nearly 200mV, no other…

  • Designing Current logger with ACS712 + AD7678 + AD8021

    Can anyone advice me how to connect these 3 component to build up a PC Current logger.

  • RE: EVAL-AD7687-PMDZ with Arduino

    I have been testing the board and have seen that Vout of the ADP7104 is 1.8V. This is the voltage fed into the AD7678 which works from 2.5V-5V, so it seems like there is a problem there. Can anyone confirm please.

    ty

  • ADC7762 on board differentail amplifier

    I am seeking performance specification for the on-chip differential amplifier on the ADC7762, in particular the maximum and recommended voltages for VinA+ (Pin 19) and VinA- (pin 20).  The data sheet appears to be silent in this regard.

    In previous designs…

  • RE: Is it a real breakthrough to remove the input voltage range limitation of IA

    Hi Jebas,

    PLease see attached list of the ADIs some of the latest differential ADCs with less tahn 2 LSB INL error. I have short listed this ADCs for DAQ systems application. I have included in the column on the file the throughput rate and full power…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…