• AD7676 Read data error

    STM32 connected with AD7676 for SPI。  this my SCH。  this is my code,read data is next picture。  I don't know why like this。AD7676 have driver code example? Thank you。

  • AD7676 with AD8021 drivers

    We have a telemetry deck that uses AD8021s as a single-ended to differential driver for an AD7676 PulSAR ADC as documented in the AD7676 data sheet.  We want to make sure that when using +/12V supplies for the AD8021s, their inherent current limiting is…

  • AD7676 interface to ADSP-2136x

    In EE248 and in the attached SW it says that "the SPORT must be configured initially for a serial word length of 15 bits". After reading two words from AD7676 the word length is then modified on-the-fly to 16 bits.

    There's not given any explanation…

  • AD7676 interface to ADSP-2136x

    In EE248 and in the attached SW it says that "the SPORT must be configured initially for a serial word length of 15 bits".

    After reading two words from AD7676 the word length is then modified on-the-fly to 16 bits.

    There's not given any explanation…

  • RE: AD7671 interfacing with ADSP21369 using SPI protocol for SERIAL mode

    Hi,

    Sorry for the delayed response.

    We suggest you to refer the EE-248 application note,which is for explains  how  to  interface  AD7676  ADCs  in  master  serial  mode  (internal  discontinuous  clock)  to  ADSP-21365  SHARC®  processors.


    Application note: www.analog…

  • AD7656 power supply anomaly

    Hi all -

    We are using two AD7656 6-channel 18-bit converters on a new product.  We have an unexplained observation on the power supply of the prototype boards.  Here's an overview:

    AD7656 power supplies (all voltages nominal)

      VDD = +15

      VSS = …

  • RE: SHARC(21366)  SPI Emulation using Flag pins

    Hi,

    It would be hard to emulate SPI using Flag pins as you need to maintain timing relationship between clock and the MISO ,MOSI. You will need to toggle the flag pins everytime the Clock and data needs a state change. This becomes cumbersome. You could…

  • RE: Is it a real breakthrough to remove the input voltage range limitation of IA

    Hi Jebas,

    PLease see attached list of the ADIs some of the latest differential ADCs with less tahn 2 LSB INL error. I have short listed this ADCs for DAQ systems application. I have included in the column on the file the throughput rate and full power…