• RE: Can AD7655 really sample at 1 MSPS?

    Is this sampling rate of [1MSPS (AD7655-EP) ] / [0.5MSPS (AD7655)] per channel or combined spec of 4 channels?

    PS: Unable to come to conclusion after thorough reading of datasheet as well.

  • AD7655出现非线性问题

    我在使用AD7655过程中,出现非线性,基准REF使用2.5V,输入电压幅度0-5V,当输入电压超过2.6V读取的AD值就出现突跳。原理图都是按照DEMO板画的。

  • RE: AD7655 return's 0xffff

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • Chip similar to AD7655

    Do you recommend any type of ADC similar to AD7655 with higher sampling rate

  • 关于AD7655的REF

    此芯片有三个基准引脚:REF(引脚37)、REFA(引脚43)、REFB(引脚42)。在我看来,REFA(引脚43)和REFB(引脚42)分别用于通道A和通道B,它们可以使用不同的电平,如果这样,是否应连接REF(引脚37)?或者说,如果使用REF(引脚37),是否意味着通道A和通道B将使用REF(引脚37)提供的同一基准电平。能否提供这些REF的推荐连接,或者您是否有AD7655的EVB原理图?我只有AD76xx的原理图,从中难以看出如何配置AD7655的这些引脚。

    Attachments…
  • ad7655总是烧坏

    我是用fpga来控制ad7655的

    前置电路用的是,ad8021接成电压跟随器的方式。ad8021是正负12V供电。其中4号脚与5号脚的电容,按照demo板上的说法,用的是NPO的。

    参考电源用的是,ad780,电容也是用的低ESR的。

    ad8021之前,我们加入了10kv的ESD芯片,作静电保护。

    ad7655与fpga之间的cnvst信号,我也加入了50Ohm的电阻用来提高EMC的抗干扰能力。

    芯片,我让它工作在,并行通信模式,四个通道可以采集数据,1Mbps的转换模式(2us,一次数据转换周期…

  • RE: AD7655 9mv output exist when tie to the GND

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD7655 does not convert analog input in normal mode!

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD7655芯片工作一段时间后异常

    AD7655芯片工作一段时间后异常,工作环境如下:

    AVDD/DVDD-5v

    OVDD-3.3V

    REF/REFA/REFB-2.5V

    和B芯片共用16位数据总线,两芯片片选互斥。

    上电后工作正常,B芯片输出数据有波动情况下,一段随机时间后(一般读取总线频率1ms的情况下,30分钟后),AD7655芯片工作不正常,不正常的表现如下:

    BUSY引脚持续高;

    AVDD供电变为4.7V;

    AD7655芯片温度急剧升高;

    除非重新上电,否则AD7655一直保持该故障状态。

    在不读取B芯片数据的情况下…

  • AD7655无法正确得到A2和B2通道数据

    AD7655可以得到A1,B1通道的数据,无法得到A2B2的数据。

    电路设计如下:采用并行数据输出,连续采样。CS和RD接地。BUS和EOC悬空。AD7655的其他控制信号均由FPGA提供。

    实验现象如下:

    将A0=0,可以正确得到A1和B1数据;将A0=1,可以正确得到A2和B2数据。

    但是A0输入一个连续高低点平后,希望正确得到A1,B1,A2,B2的数据。但是发现A1和A2都是同一个数据(是基本等于A1的值);

    B1和B2都是同一个数据(是基本等于B1的值),也就是数据线上的数据都是A1和B1的值…