The AD7616 and AD7616-P have similar functionality, with a few key differences.
你用的芯片是AD7616还是AD7616-P, AD7616-P的并口时序兼容控制器的时序会更好。
After configuring the sequencer in software mode, a “dummy” conversion is first required in order to latch the configuration into the ADC. After one dummy conversion has been performed, the ADC is fully configured for use with the sequencer and no further…
The Page no 40 in the attached datasheet contains pseudo code for the CRC calculation . Can anyone explain it bit elaborately
Hello, I'm looking for a multi-channel (>=16) ADC with 0..16V inputs. The project is telemetry system for an old car with analog sensors. It seems that AD7616 (EVAL-AD7616) might fit but there is a little misunderstanding about it.
Manual says…
Hi,
i'm trying to use ad7616 for new design which is having more than 80 channels on 2FMC's and i need to design for synchronized data... can anyone tell me how to use this IC for synchronization purpose without any clk or sync pin's.
and…
HI !
我想使用AD7616-p 通过SPI来控制AD的采集,想使用芯片的2串行来实现。但是不清楚怎样连接SPI,是连接一路SPI还是两路。若是两路的话,时钟和片选怎样连接设置。
Do i need an Isolation ADUM to separate AD7616 serial interface from the MCU ?
Also, do i need to isolate the power for the AD7616 ?
Does AD7616 requires an external reference clock?