• AD7616-P: What are the differences between the AD7616 and AD7616-P?

    Questions:

    What are the differences between the AD7616 and AD7616-P?

    Answer:

    The AD7616 and AD7616-P have similar functionality, with a few key differences.

    • The AD7616 has both serial and parallel digital interfaces
    • The AD7616-P has a parallel only…
  • AD7616-P FAQs

    Question:

    The analog input diagnostic channels are showing an unexpected result for AD7616-P, what should I do?

    Answer:

    The diagnostic channels are used to check the health of the ADC and as a “sanity” check to compare other results against. If the result…

  • AD7616-P datasheet error

    CHSEL0 and CHSEL2 in table 12 of the AD7616-P datasheet need to be be swapped.

  • AD7616-P FAQ - When using the software sequencer, the first conversion result is not the expected value?

    Question:

    When using the software sequencer, the first conversion result is not the expected value?

    Answer:

    After configuring the sequencer in software mode, a “dummy” conversion is first required in order to latch the configuration into the ADC. After…

  • AD7616 channel synchronization???

    Hi,

    i'm trying to use ad7616 for new design which is having more than 80 channels on 2FMC's and i need to design for synchronized data... can anyone tell me how to use this IC for synchronization purpose without any clk or sync pin's.

    and…

  • About multi channel synchronization with AD7616

    Hi,

    i'm trying to use ad7616 for new design which is having more than 80 channels on 2FMC's and i need to design for synchronized data... can anyone tell me how to use this IC for synchronization purpose without any clk or sync pin's.

    and…

  • AD7616 conversion reading

    Hello,

    I'm using the ad7616sdz board. I'm trying a digital interface self-test. Read out the reset default values of registers correctly. write 0x86BB to the channel register (0x03) for self-register. Subsequently, read the channel register value to make…

  • ad7616 unipolar mode

    The ad7616 datasheet mentions it works in bipolar mode

    True bipolar: ±10 V, ±5 V, ±2.5 V

    does it support unipolar analog input 0 - 10v?

    Thanks,

    Shahul

  • AD7616 IP

    Hi,

    I want to know if AD7616 IP is only suitable for Hardware(Serial or Parallel) Mode? Is it suitable for Software(Serial or Parallel) Mode?

    Thanks for replies in advance.

  • AD7616

    HI !

          我想使用AD7616-p 通过SPI来控制AD的采集,想使用芯片的2串行来实现。但是不清楚怎样连接SPI,是连接一路SPI还是两路。若是两路的话,时钟和片选怎样连接设置。