• 2009-03-09 16:16:14     Mounting jffs2 partition

    2009-03-09 16:16:14     Mounting jffs2 partition

    Steven Vacca (UNITED STATES)

    Message: 70622   

    I am having troble getting my jffs2 partition mounted.

    My Environment:   bf537 dev unit, m25p128 FLASH

    --------------------------------------

    Kernel boot-up…

  • Choosing adc LTC2335-16 or LTC2358-16 for "music product"

    I'm i the process of choosing an adc for a music project, the adc role is to read analog "control voltages" or "cv" that range between -10 and +10 volts, the data is used to set pitch of oscillators and control other parameters. First i chose the LTC2358…

  • Choosing adc LTC2335-16 or LTC2358-16 for "music product"

    I'm i the process of choosing an adc for a music project, the adc role is to read analog "control voltages" or "cv" that range between -10 and +10 volts, the data is used to set pitch of oscillators and control other parameters. First i chose the LTC2358…

  • 2011-03-16 01:16:36     SD card with BF53x

    2011-03-16 01:16:36     SD card with BF53x

    Sergio Morales (COLOMBIA)

    Message: 98955   

    HI,

    I'm trying to use the SD card driver over SPI, this is the connection used:   wiki.linuxencaja.net/images/6/63/Sch_uSD.jpeg

    I have kernel version 2010R1. Reading…

  • 2008-02-01 16:16:34     API for GPIO Wakeups

    2008-02-01 16:16:34     API for GPIO Wakeups

    Christopher Harrsen (UNITED STATES)

    Message: 50582   

    I would like to use the API for GPIO wakeups. This is a kernel space API. Does this mean I have to compile my application to run in Kernel space. How do…

  • RE: Internal Reference characteristics - LTC2326-16

    I can confirm that the temperature coefficient is in ppm/deg.C.

  • 2010-04-16 14:16:51     New to uClinux and Blackfin

    2010-04-16 14:16:51     New to uClinux and Blackfin

    Matthew Sacrey (UNITED STATES)

    Message: 88529   

    Hi

    I'm working a class project involving a BlackFin 548 evaluation kit. My tea inherited the project from a previous year's group, who installed uClinux…

  • 2008-02-11 16:16:27     Getting Started with Skyeye & bf533

    2008-02-11 16:16:27     Getting Started with Skyeye & bf533

    Michal Steyn (AUSTRIA)

    Message: 50910    I am new to Skyeye and uCLinux. I am working on a project using a Blackfin bf533 processor.

    I am trying to configure my system but I cannot get any…

  • 2010-06-16 16:14:47     2009R1.4 netflash w/ HMAC_MD5 doesn't build

    2010-06-16 16:14:47     2009R1.4 netflash w/ HMAC_MD5 doesn't build

    Andrew Kohlsmith (CANADA)

    Message: 90344   

    It can't find openssl/sha.h. The file exists both on the host (/usr/include/openssl/sha.h) as well as in the uClinux-dist (lib/libssl/openssl…