兄弟你好!你的板子是STM32还是跑Linux的板,我目前用的是IMX6ULL的板子,也是6通道的AD7606,采用SPI输入输出,对于驱动移植应用程序开发这个不会搞,能不能帮忙看看
兄弟你好!你的板子是STM32还是跑Linux的板,我目前用的是IMX6ULL的板子,也是6通道的AD7606,采用SPI输入输出,对于驱动移植应用程序开发这个不会搞,能不能帮忙看看
Q: Are there special grounding considerations for the AD7606?
A: At least one ground plane should be used. It can be common or split between the digital and analog sections. In the case of the split plane, the digital and analog ground planes should be…
我自己做了一块ARM板,内核是4.1.15,采用了AD7606-6模块和ARM板的SPI接口连接,同时按照手册里的要求,将IMX6UL_PAD_GPIO1_IO02 GPIO1_IO04 GPIO1_IO093个GPIO口作为BUSY、RST和CVS引脚。前期看官方文档没有什么思路,有知道怎么解决的兄弟吗?有偿解答
qq:962081978
继续上一次追问 2.240V直流电压,经过10KΩ电阻分别连接在IN0~IN15,状态控制引脚为
(CE=0 UPDATE=1 CLK=1 D4=1 D3=0 D2=0 D1=0 D0=0 A2=0 A1=0 A0=0 CLK=0 delay_us(1) UPDATE=0 CLK=1 RST=1 输入IN0对应输出OUT0,OUT0电压2.241V),
(CE=0 UPDATE=1 CLK=1 D4=1 D3=0 D2=0 D1=0 D0=1 A2=0 A1=0 A0=1 CLK=0 delay_us…
Hi Anurag,
The actual sampling rate you can achieve is determined by the time for each LED. In your use case, if you set the sampling rate for 1 kHz, you will have less than 1 ms to finish data acquisition for all 6 LEDs. The 1 kHz sampling rate is achievable…
Hi,
Apologies if this seems a dumb question. Can I used the AD5840/5941 to perform Electrochemical Impedance Spectroscopy on a battery of cells?
I want to test a 6 cell lithium battery, as a minimum across the battery of 6 cells, ideally use more devices…