• Schema connection DAC AD7538

    I use DAC AD7538.
    Where is pluged blocking capacitor?
    What type capacitor (aluminium electrolytic, tantalum, ceramic) is needed?
    What is nominal voltage capacitor?
    Should is use ferrite bead?
    Should is use choke?
    Temperature work DAC maximum 55 grade. Current…

  • generation  sinusoid with help AD7538

    I design electrodrive micromotor. Micromotor supply 3 sinusoid with
    variable-amplitude and frequency (0-53 Hz or 0-106 Hz; 540 point on
    period). Configuration chanel(1 faze): DAC AD7538 with AD8675,summarize
    AD8675, filter 1 or 2 degree on AD8675, power…

  • RE: Resistor feedback DAC AD7538KR.

    Hi ,

    The feedback resistor is 6 kOhm typical. 

    May I know what is the application for AD7538? May I also know your requirements? If suitable, we have newer MDACs which may be used for your application.

    Cheers,

    Ivan

  • RE: How can increase the WRL after using max wait cycle.(for TS201)

    Hello jeyanthi,

    Thank you for technical support . YES !! Now  my custom Tiger-sharc(TS201) board is  working fine .

    Problem :

       AD7538 , 14 bit DAC need 240 nsec where as TS201 processor generating maximum 145 nsec WRL pulse

    even setting maximun WAIT…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…