• problem of AD7490

    想請問如何使用AD7490  有verilog 的範例嗎

  • AD7490  driver

    I want to interface AD7490 (SPI) with Nrf51822 in current development project.

    So, please provide SPI Driver or SPI Driver implementation steps for AD7490.

    Awaiting for your reply.

     

    Thanks & Regards

  • AD7490: Range Bit

    I want to use the 16 Channel of the AD7490 to convert some 2,5V Vin and 5V Vin
    by setting Range Bit of the Control Register.

            e.g.    Channel       Analog Input Range
                    0               0 to REFin            
                    1               0 to 2 x REFin          Wating time for Range
    switch ?
                    2               0…
  • AD7490 Sampling Rate & Artifacts

    Hello,

    I am testing a design with an AD7490 and I'm a bit unsure on how to determine the sampling rate. Given VDD of 5V, per the datasheet a 20 MHz SCLK should be equivalent to a 1MSPS sampling rate. Does that mean it's a 20:1 ratio for the sampling…

  • EVAL-AD7490 hardware schematic

    Hi ADI Expert,

    I am evaluating the EVAL-AD7490, but without any hardware schematic file in the web site, may I have your help to assistance? thanks.

    Best regards.

    Ray.

  • question on ad7490

    How do you do dear specialists.

    In new product our company put into use 16-canal ADC AD7490.

    On pilot models of the product I faced with the following problem:

    the given channel ADC differ under alike input voltage.

    The Register of management ADC…

  • AD7490 SPI Issues

    Hello I am trying to configure my ad7490 with my Arduino Due. I have searched and searched and cannot find the issue with my circuit. I am posting the code below: 

    In the code I try to get the value of  a single channel. 

    I think the problem is either a…

  • serial timing of the AD7490

    Hello!

    Currently I am working with the AD7490 and trying to get it run with SPI. I am using an USCI-module of an MSP430F5659 to establish the serial communication.

    By studying the datasheet of the AD7490 the following question came up:

    The AD7490 requests…

  • AD7490 SPI Driver Support

    Hi,

    I want to interface AD7490 (SPI) with STM32F205ZE in current development project.

    So, please provide SPI Driver or SPI Driver implementation steps for AD7490.

    Awaiting for your reply.

    Thanks & Regards

    Santhosh Kumar B

  • AD7490 EVAL-SDP-CB1Z

    Hello

    One of the customer wants to evaluate AD7490.

    According to UG-446, EVAL-SDP-CB1Z is required to evaluate AD7490.

    http://www.analog.com/media/en/technical-documentation/user-guides/EVAL-AD7490SDZ_UG-446.pdf

    But we can't find out the order guide…