使用AD7472时,模拟输入电平最大达到5V,怎么接入AD7472,如果用运放,我只有一个单电源,怎么接
hello guys, Im new here. i hope u can help me how to write coding in c using avr microcontroller to control the external ad7472 conversion, my supervisor ask me to do that. the problem is i dont know how to control the cnvst because i never used avr.…
The Data sheet for AD7470/AD7472 says acquisition time is *minimum* 135[ns] in "Specification" section and then in the "Timing Specfications" section says this number is a max. I assume this is an error or am I missing something?
Hi jcolao,
Thank you for the reply. I understood you do not have the ibis model for AD7472.
Then, how about the following questions? Could you support it?
Both high and low sides of the totem-pole are used FET or transistor? Is there a resistor on…
Hello guys, I'm currently working on AD7472. according to the datasheet the REF IN is 2.5V which means the VIN can only varies from 0 to 2.5V. But i want to change the REF IN FROM 2.5V to 5V so that the ADC can read the VIN from 0 to 5V. How do u guys…
关于AD选型过程中,看到ADI出了一些针对直接射频采样的高速宽带ADC和DAC,比如AD9625和AD9144,最大采样率可以支持2.5GSPS和2.8GSPS. 我一直有个观点,就是SDR的一个目标是AD/DA尽可能的去靠近天线,这两款芯片组合起来可以对 GHz频段信号进行直接射频采样和直接射频合成。以前我也一直觉得,要想对更高频率进行AD转换,就需要更高采样率的ADC,可我最近研究了带通采样(欠采样)定理后,采样速率只要满足带通采样速率的要求就可以 了,这样的话,ADC的采样速率只和接收信号的带宽有关系…
Hi Postino,
Here are some list of ADC that could be suitable for your application. You may also wanted to check the ADI website and do a parametric search and put in parameters on the ADC that you wanted to search. Please refer to the link below.