• AD7648 : slowest fclk and affect

    Hello,

    I have a question about AD7468 SAR ADC.
    The AD7648 has a specification about fclk as followings. (tabel-4 of the datasheet)

    Parameter     Limit at TMIN,TMAX     Unit        Description
       fSCLK             3.4           MHz max         Mark/space ratio for the SCLK input is 40/60 to 60/40.

  • Ultra low power data collection - reading strain guage

    I have a customer that needs to digitize the output of a strain gauge.  Their power source can vary from 1.6 to 3.6V and is capable of supplying no more than 200 uA.  Ideally, they want to use a differential input A/D and want a SPI output.  Sample rate…

  • RE: ADC used for single-pulse conversion

    Hi Postino,

    Here are some list of ADC that could be suitable for your application. You may also wanted to check the ADI website and do a parametric search and put in parameters on the ADC that you wanted to search. Please refer to the link below.

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…
  • ADI芯片辨识、型号查找

    看看截图: