Hi,
Is there any documentation for the C++ driver that is available for download for the AD74413R?
Thanks
Hi,
Is there any documentation for the C++ driver that is available for download for the AD74413R?
Thanks
Hi,
1. I want to implement the below mentioned circuit in current input (external powered mode)
Is it possible to sense the current across Rsense, when internal 200K ohm connected to VIOUT_N is disabled ?
2. In AD74413R, Is it possible to sink and source…
Hi,
Apologies for missing this item. I am not sure if it still relevant to you that this question will be answered, However, we are clearing up some open items in our community and ensure that any query is located on its proper community as others who have…
Hi,
Apologies for missing this item. Looks like it was transferred from a different community.
First, I'm afraid I cannot find any available reference circuit that will match your requirements as it is a very specific request. However, I think you can…
Hi,
Apologies for missing this item. I am not sure if it still relevant to you that this question will be answered, However, we are clearing up some open items in our community and ensure that any query is located on its proper community as others who have…
Would you please help to provide EVAL-AD74413R DSN file. Thanks~
Hi,
1. The current Input loop powered range is 0 to 25mA
2.
The Current INput Loop powered & externally powered functions come with a selectable additional input impedance to ensure that a minimum of 240Ohm is achieved to be compliant with the HART spec…
Hi Dmitry,
based on the information you told me, I can suggest you, that you need to consider following:
From datasheet is obvious that SPI read process of AD7124 is completely different from AD74413.
Key differences are how SPI access, especially during…
Hi,
Unfortunately, only the C driver is available at this time. We are working on preparing No-OS & linux drivers but I do not have a delivery date for this just yet.
Apologies for the inconvenience. If you need help with specific sequences when programming…
Hi,
Apologies for the delay.
In the default system configuration (as per figure 39 in the AD74413R datasheet), differential voltage measurement cannot be supported.
In this configuration, SENSEHF and SENSELF complete a differential voltage measurement…