• AD7415 I2C

    Hi

    I'm a DFAE in Japan. Our customer give us a question. There is a MOSFET inside SDA pin of AD7415. On the other hand, is there NO MOSFET inside SCL pin of AD7415? According to Table 3, we couldn't see Open-drain output about SCL as follows.

  • IBIS model for AD7415

    Hello,

    My customer use AD7415 for wireless application and  requests IBIS model of AD7415ARTZ-0500RL7.
    Would you provide IBIS model?

    Thanks and regards,
    Makio

  • AD7415 I2C again

    Hi,

    Could anyone help my question of below link instead of Karen who is located philippines where is critical situation due to COVID-19?  Our customer is waiting for it.

    https://ez.analog.com/temperature_sensors/f/q-a/162919/ad7415-i2c

    Regards,

    Hiroyu…

  • AD7415 Absolute Maximum Ratings 

    Hi all,

    Here is the Absolute Maximum Ratings in the datasheet at AD7415,
    SDA Input Voltage to GND : −0.3 V to +7 V
    SCL Input Voltage to GND : −0.3 V to +7 V

    This means that SDA & SCL are not related to VDD ?

    "−0.3 V to VDD + 0.3 V" is correct ?…

  • AD7415: Long-term stability data

    I would appreciate if you could send me the information concerning the
    long-term stability of AD7415 temperature sensor.

     

    Unfortunately we don’t have any long term stability information on file for
    AD7415.
  • AD7091R-5 and AD7415 SDA, SCL

    Hi

    I'm DFAE in Japan. Our customer connect AD7091R-5, AD7415 and others with I2C interface in the system. When the system is powered off, both SCL and SDA are into LOW. His end-user suspects that there is an IC in his circuit that pulls those signals…

  • AD7415: ESD protection of SDA and SCL pins

    Hi,

    The AD7415 have I2C interface (SDA and SCL).

    Do these pins implement ESD protection?

    Also please tell me the equivalent circuit.

     

    Best regards,

    Makio

  • How Can AD7415 device transients think it is a wrong I2C address?

    I have an embedded application using AD7415-0 part.   I have 4 instances (in perhaps 2000 devices) where temp sensor stopped responding it I2C commands.   Probing on the I2C command from the master, it all looks good.   On 3 of the 4 devices, power cycling…

  • twi interfacing problem....

    Hi,

    i am using AD7415 temperature sensor in floating mode of AS. i followed the instructions as per the hard ware reference to interface  an i2c device(AD7415). but it was not generating clock. following attachment consists C code. i am using core clock…

  • AD7405-1 no ack on second Byte..

    Hi All,

     

    I'm using a AD7415-1 (I2C interface) and the timing it at 5usec or 200KHz clock.

    After power up (aprox 1second) I'm not able to setup the AD7415-1 correctly.

     

    Following the datasheet information I'm starting by seting up the Configuration…