FAQ
Hi Jatin,
The AD7400A and the AD7401A parts are our parts that are targeted at shunt current monitor applications.
They accept signals in the +/-250mV range and have in-built isolation based on ADIs iCoupler technology.
The output of the AD7400A and…
Hi Ignacio,
Sorry for getting back late. We have an analog isolator circuit which you may want to consider. It is implemented by using AD7400A, an Isolated Sigma-Delta Modulator. Here is the link of the reference circuit:
混合信号处理器新标杆ADSP-CM40x在电机控制中的应用 by ADIForum
下一代混合信号处理器的标杆产品ADSP-CM40x系列最大的应用之一就是电机控制。这里分享ADSP-CM40x在电机控制中的应用资源供大家学习参考,也欢迎有电机控制应用需求的筒子们跟帖讨论、提问。
伺服与电机驱动器设计人员需要高度精确的闭环控制以改进产品的能效和性能。全新ADSP-CM40x 系列混合信号控制处理器集成嵌入式双通道16位ADC,精度高达14位,同时还集成240 MHz浮点ARM Cortex
-M4处理器内核…
Hello,
I am a student of the Engineering School of Fribourg in Switzerland. I’m using
a EVAL-CED1Z evaluation kit in combination with a AD7400A Delta-Sigma Converter
for a school project. I need to know if it’s possible to store the bit-stream
(directly…
Hi Natanel,
The internal clock on the AD7400 and AD7400A is used to clock the converter internally and also to allow the user to clock out the data bits from the modulator into an FPGA for example or other receiving device.
This clock typically runs…