• RE: Save RAW datas from EVAL-AD7400EDZ ?

    Hi Mickael-

    I moved your question about the AD7400 Evaluation board to the Precision ADCs community.  Someone here should be able to assist you.

    Regards,

    AndyR

    EngineerZone Community Manager

  • AD740x maximum input to output delay

    What is the maximum input to output delay of AD7400/AD7401 provided that a 4 MHz clock signal is provided? Is there a certain way to control exact sampling point?

  • medical ADC isolation

    Hi

    I would like to read temperature from thermistor connected to catheter (medical device)

    using the following thermistor P12358CT-ND, THERMISTOR NTC 10K OHM 5% 0201

    MCU is arduino uno board

    after reading I found the AD7400 and  AD7400A and have a…

  • RE: ADC evaluation board choose

    Hi Yake,

    I have attached a list of some of the ADCs that fit your criteria of 2MSPS sampling rate or higher at resolution of 12bits or more.

    You may also wanted to check the ADI website and do a parametric search (http://www.analog.com/ps/psthandler…

  • RE: High-side current sensing at 120V

    Hi Benrd,

    have you looked at the AD8212?, If you can affort to "burn" some bias current this should be a good solutiuon.

    http://www.analog.com/en/specialty-amplifiers/current-sense-amplifiers/ad8212/products/product.html

    You can also use…

  • RE: ADC 12/14BIT, >2mS/S, Parallel digital interface

    Hi Meir,

    You may  want to check the ADI website and do a parametric search to filter the product display  base form your recommended specification.

    www.analog.com/.../10169

    Here are some ADCs that might help  you start with, kindly see attched file.

  • AD7400A:  Can this device accept both differential and single ended inputs, datasheet is not clear?

    The AD7400A specifies an analog input range of +/- 200mV and a specified full
    range of +/- 320mV, which I interpret as a bipolar input. When looking at the
    abs max ratings, it can only be on the negative side GND -
    0.3V.

     

    1. The…
  • 哇哦,太阳能逆变器与摩尔定律保持一致!!!

    当小编第一次看到太阳能逆变器将与摩尔定律保持一致时,非常震惊滴,但又很期待不久的将来,广大群众能够用上太阳能,激动万分。

    先交代一下背景故事,SolarEdge是太阳能逆变器、功率优化器和模块级监控服务领域的全球领导者,自公司成立以来短短 10 年内从新初创企业一跃成为行业领导者之一。奇迹是如何发生的呢?

    SolarEdge意识到若要摆脱逆变器的这些笨重、庞大的金属元件,则需要重新思考转换过程。虽然碳化硅 (SiC) 和氮化镓 (GaN) 等新的宽带隙交换技术的出现,有望革命性地改变下一代功率转换设计…

  • Using AD7401A with SINC4 Filter with Decimation Factor 128?

    In order to increase the bandwitdh and the SNR of the acquired data we would like to use a SINC4 Filter with a decimation factor 128 instead of a SINC3 Filter with a decimation factor 256. With these measures we hope to increase the bandwidth to 150 kHz…

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…