The AD7380 is capable to perform with throughput rates over 4MSPS using the correct SCLK at 80 Mhz frequency. When the normal averaging oversampling and resolution boost are enabled, the throughput rate will slow down as the oversampling ratio increases…
The buffered 2.5V internal reference of the AD7380 is recommended to use for internal circuitry process. When this on-chip 2.5V reference is use for external circuit, it must be connected to an external buffer amplifier for example the ADA4807. The external…
Hello Jonathan,
As per your suggestion in below linked thread we have used the analog filter(capacitor based) in the setup.
https://ez.analog.com/data_converters/precision_adcs/f/q-a/536556/analog-filter-used-before-ad7380-evm
Setups are given below…
Hello Kommissar,
Do you have a power-up sequence on your application? Looking into the Abs max rating of the AD7380, the REFIO pin range is related to the VCC. Violation on this abs max rating could potentially damage the part. I good power up and power…
Question:
The AD7380 has an on chip oversampling, Why is there a need for an oversampling?
Answer:
Oversampling has been a known method of processing conversion result to improve ADC performance for SAR ADC. Putting the oversampling process internally…
Hi,
For the AD7380, conversion data, MSB is shift out as soon as the CS goes low, the subsequent data bits are shift out at the rising edge of SCLK,. Based from this figure , the recommended SPI timing would be CPOL=1 and CPHA = 0.
Regards,
Jonatha…
Hello,
In AD7380 EVM user guide one analog filter has been used (Mentioned in the first page of user guide UG-1304)
1) Kindly share details of the analog filter.
2) Also the signal characteristics used to get result as given in figure 20 of user guide…
Dear ADI,
We are planning to use AD7380/AD7381 in our products, sensing two industrial signal (+- 13.5V) simultaneously. We now stop on the choices of ADC drivers.
In the past, we are using CN0385 (AD8251 + AD8475 + AD4003) as the solution, and in using…
I checking on other ADC Driver. I ma currently using ADA4945, ADA4896 and ADA4807. Are there other recommended new ADC drivers for AD7380?
Jocs
I'm DFAE in Japan. I have a question about SCLK in 2-wire mode of AD7380 from a customer.
I think we don't need to send SCLK while SDOA/SDOB are DON'T CARE. Is it correct?
Best Regards,
Akira