• AD7367 Evaluation board

    I need information about the AD7367 evaluation board. According to the datasheet the board includes a level shifter to translate the communication signals from 3.3V to 5V. Using that level shifter, is it possible to use the SPI at 48 MHz even if the board…

  • AD7367 output coding

    Hi all,

    The output coding of the AD7367 is twos complement.

    Is it both bipolar and unipolar input ?

    : ±10 V, ±5 V,or 0 V to 10 V.

    Best regards,

    sss

  • AD7367 ADC calibration

    I am using the AD7367 and am interested in achieving better accuracy.  I am using a high accuracy external reference.  I am using the ADC in either the +/-10V or +/-5V range.

    Can I perform a one time gain and offset calibration, or would I need to do that…

  • AD7367 busy signal

    Hi,
    Our customer has a problem with AD7367. When AD7367 is powered up, the BUSY signal is sometimes High. I knew how to reset from following Q&A.
    https://ez.analog.com/docs/DOC-13462
    But RANGE0 and RANGE1 are fixed low at Customer's circuit.
    I…

  • AD7367 SPI clarification

    From the data sheet:

    "Alternatively, the CS pin can be tied to a low logic state continuously. In this case, the DOUT pins never enter three-state and the data bus is continuously active. Under these conditions, the MSB of the conversion result for…

  • AD7367 - Input going down?

    Hi!,

    I'm working with a AD7367. 

    There is a oscilloscope screenshot.

    In blue: CNVST.

    In yellow: VA1.

    In pink: VA2.

    Why when VA1 or VA2 is selected, the other "goes down"?

    Could it be a "internal" (IC) problem?

    On the other…

  • AD7367 SERIAL INTERFACE

    Hello,

    I have three questions about AD7367 from our customer.

    When 14SCLK is input with CS pin set to low level, the A-data is output from DoutA pin.
    After, setting CS pin to the high level again, and CS pin is set to the low level agein, will the A-data…

  • AD7367-5 circuit diagrams

    When I used the AD7367-5 for a single-end  bipolar range-±5V analogue input signal,I couldn't 100% be sure that could that chip work in the single-ended model,since  Figure 21 about typical connection diagram in the data sheet AD7367 has some conflict…

  • Designing a PCB for AD7367

    I'm working on a design with the ADC: AD7367 and I have some questions about how to route the PCB, more concretely, how I have to join AGND and DGND. I was reading the reference design, but I have 6 layers instead of 4 layers.

    My stack up has 6 layers…

  • Using AD7367 eval board in Design

    Hi ,

             I am using AD7367 ADC evaluation board along with EVAl-SDP-CBZ controller board. I want to use this setup directly in my system. The software came with the board do not allow to be modified as per my requirement. In this connection I request you…