您好,AD736的CAV引脚为什么接这种电容,+一端接的是CAV引脚,另外一端接的是-VS。我拆下来用电桥测了是1UF容值,但是不确实定的是薄膜电容还是电解电容?
因为图片中标出了正极+。网上说薄膜电容没有极性。还是电解电容。但是电解电容没有这种形状的。很疑惑。希望得到大家的回复,谢谢了!
您好,AD736的CAV引脚为什么接这种电容,+一端接的是CAV引脚,另外一端接的是-VS。我拆下来用电桥测了是1UF容值,但是不确实定的是薄膜电容还是电解电容?
因为图片中标出了正极+。网上说薄膜电容没有极性。还是电解电容。但是电解电容没有这种形状的。很疑惑。希望得到大家的回复,谢谢了!
Dear Sir,
Can I able to use AD736 for Both AC Input and DC Input?
Is it possible to use for both AC and DC Signal Sensing?
I tested with AC Singal Conversion true RMS to DC working properly, for DC signal Input I am not getting any output.
Please suggest…
Hi,
As I followed the application note and the datasheet to test the real rms-to-dc converter circuit, I first chose the AD8436 because of its high operating frequency. However the simulation in LTspice always come the similar errors no matter which circuit…
Can the use of ad736 solve the erratic display osaro CT current by pic microcontroller?
Original Question: problem simulating AD736 in ADIsimPE by suryadeopa
simulating AD736.
I was trying to simulate AD736 rms to DC converter for 200mV input for fastest settling time. I have attached the circuit below. I might have made mistakes in selecting…