• About AD7356 real-time

    The control system drives and outputs the pulse signal, and then informs the monitoring system to collect the pulse signal through the external expansion AD7356. Due to the communication delay, the AD7356 cannot collect the pulse signal. How to solve…

  • EVAL-AD7356 capacitors C1, C2, C3 and C4 value

    Hi,

              There are four capacitors C1, C2, C3 and C4 on the Eval_board not fitted, can you please let me know what should be the value of these capacitors?

    When the clock input (SCLK) increases more than 50 MHz, the output data on SDATA disappear, but…

  • About AD7356. Error in data acquisition

    Recently, I am using AD7356 to collect data. The hardware circuit is correct. Maybe my FPGA program is wrong and there is bit error in the acquired data. I used altera's FPGA and observed AD converted data using signaltap on quartus II, and the results…

  • RE: AD7356 Evaluation Board

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Micro-Controller for AD7356

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD7356 Evaluation Software ,Save (Sample Data)

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Using Single ended analog input in AD7356

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Help setting up software for EVAL-AD7356  +  CED1Z

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD7356中Vdrive电压由谁提供?

    AD7356中Vdrive电压由谁提供,是单片机,还是说要用AD7356的驱动芯片来提供。这款芯片可以直接接SPI使用吗?还要请问以下AD7356的数据采集是采集一次直接发十二位数据还是分两次发?

  • 请教:AD7356的单次数据采集问题

    问题:AD7356的ADC开始转换是以SPI接口的CS信号的下降沿开始的。根据adc的采样率5MHz要求,cs信号有最小时间间隔要求,是200ns。那么cs信号有没有最大时间间隔要求?比如,通过MCU软件控制ADC进行不定时的单次采样,可能数秒钟1次或者连续以200ns时间间隔采集8组数据取平均等突发式的采集。这里不太需要考虑功耗,所以ADC处于normal模式,不进入待机状态等。这种单次采集相对于固定周期采集(比如固定1MSPS)会有损失吗?或者会出现工作异常吗?比如第1个采集数据不正确等。其他带有类似SPI接口的ADC…