Hi ,
I would like to ask quick questions on the AD73360 just for confirmation purpose.
Quick replies would be appreciated.
Q1. Where are the timing reference points on SCLK, SDOFS , and so on.
-- At the 50% level of the swing of each signal?
Q2: Assiming…
I am using AD73360L for my application. but the problem with this ADC is that it does not specify its variation with respect to temperature. for my appliocation temperature effect is signifcant. i want to know whether and how does this chip get affected…
I'm using a 73360 to read six sensors continuously. My problem is determining when sensor 1 is being output.
From looking at the timing diagrams in the datasheet, I see no output signal that differentiates which sensor is being output.
This must…
Hi, all
I have a board with BF518 & AD73360.The board is same with zhe BF518EZBRD except the AD. We use AD73360 instead of AD7266.
I want to sample message with this board.Now I need to write a driver of AD73360 to match the uClinux.I hope someone…
Hi all,
I hope I'm posting this in the correct section...
I am looking for an A/D converter which has all the features of the AD73360 (simultaneous sampling, daisy chain, high-gain PGA, 16-bits or higher, etc). But with an SPI interface. The AD73360…