• AD73322L: Frequency response

    I have a question relating to the operation of the AD73322L frequency response.

    I am testing the device with Sine wave tones ranging across the voice band
    between 300Hz and 3400Hz and
    Am finding that with a sampling rate of 16Khz, I am…
  • AD73322/AD73322L compatibility

    Can I use the AD73322L as a replacement for the AD73322 and is it pin and
    software compatible?

     

    The AD73322L is a cost reduced version of the AD73322 and is fabricated on a
    0.35um process. In 3V applications, the AD73322L is pin for…
  • AD73322L: symmetry within the sigma-delta modulator

    AD73322L datasheet:

    Word growth in the decimator is determined by the sampling
    rate. At 64 kHz sampling, where the oversampling ratio (OSR)
    between sigma-delta modulator and decimator output equals
    32, there are five bits per stage of the three-stage Sinc3…

  • AD73322L Digital loop-back mode

    Hi,

    I need to be able to enable/disable AD73322L digital loop-back mode feature for
    diagnostic purposes while the device is running.

    The device is configured in mixed mode and is properly working with audio
    samples and control words. I am able to…

  • Can I adjust Frequency Response of AD73322L?

    Can I adjust the output frequency response of the AD7332L? I am getting a quick roll off starting at 1.2KHz with a 3db down point at around 2KHz and would like to extend that cutoff to 4K or so. I understand that this is a “telecom specific” Codec so…

  • 2010-04-26 09:24:00     Audio function on BF537 ez-kit

    2010-04-26 09:24:00     Audio function on BF537 ez-kit

    Bo Li (CHINA)

    Message: 88902   

    Dear guys,

    BF537 Ezkit has ad1854 and ad1871. I want to realize a simple 'talkthrough' application before further work. But I met some problem. By default they are…

  • RE: SLIC interace with Blackfin

    Hi,

    We have an application note EE-193 describing the interface of  ADSP-BF535 BlackfinRegistered Processor to the AD73322L Codec. And  AD73322L is particularly suitable for a variety of applications in the speech and telephony area, including low bit rate, high…

  • How to generate interrupt using external clock and frame sync?

    DSP: 21489

    Audio Codec:AD73322L

    Operation mode: Using AD73322L generate bit clock,frame sync.

    Question: The DMA is work,but no interrupt generate.When using Internal clock the DMA interrupt enter. Why & How to do?

    Thanks.

    Init code:

    section…

  • ad73322 adc sometimes 0->65535, sometimes 65535->0, per unit basis

    Hi all,

    I have a unit which uses the ad73322L analog front end. It works very well in a 3-chip cascaded formation. If I have, for example,

    8 units produced, the 1st of the 3 cascaded 73322 chips on 4 of the units will convert audio input A/D producing…

  • TAGS LIST: Audio

    AD8024
    AD8509
    AD8511
    AD8531
    AD8532
    AD8534
    AD8565
    AD8566
    AD8567
    AD8614
    AD8644
    ADD8504
    ADD8710
    AD8519
    ADSY8401
    AD8529
    AD1870
    AD1871
    AD1877
    AD1974
    ADAU1977
    ADAU1978
    ADAU1979
    ADAU7002
    SSM2602
    SSM26…