• AD73322/AD73322L compatibility

    Can I use the AD73322L as a replacement for the AD73322 and is it pin and
    software compatible?

     

    The AD73322L is a cost reduced version of the AD73322 and is fabricated on a
    0.35um process. In 3V applications, the AD73322L is pin for…
  • AD73322: CD measurability

    I want to make measurements at the tachometer output from dc-motors. This
    signal is a dc-voltage with ac-parts (if the motor accelerate or stop). The
    bandwith is therefore dc-max 2kHz. Can I use the ad-inputs of the ad73322 for
    such a…
  • AD73322 Patch

    Where is the AD73322 Patch located on GIT?

  • AD73322: Vref transfer function

    Are the Vref directly connected to internal non inverting input of the op, or
    this is an principle schematic  and the output op signal are only biased with 
    Vref.
    In other word is the transfer function of the input stage :


    a)Vout…
  • Power supply AD73322

    Hello! Can I use the AD73322 with AVDD = +5 V and DVDD = +3.3 V? Thanks, Sergey

  • AD73322 in newer kernels

    Hey gang,

    I'm experiencing the same issue that was reported here:

    https://blackfin.uclinux.org/gf/project/uclinux-dist/forum/?action=ForumBrowse&forum_id=39&_forum_action=ForumMessageBrowse&thread_id=42625

    Basically, there appears to…

  • Interfacing AD73322 to ADSP-21369

    We are wanting to connect a AD73322 to the SPORT

    Just wondering if anyone has done this before or can just check what i plan on doing is okay.

    From the codec I want to connect

    CODEC_SDI to SPORTx–0_DA_I/O

    CODEC_SDO to SPORTx–0_DB_I/O

    CODEC_SCLK to…

  • AD73311/AD73322 application circuit and layout

    Hi

    I would like to have a information about EVAL-AD73311 or AD73322.

    I know Eval-AD73311 is obsolete.

    But we don't have any information about actual Layout and application circuit.

    Please help us.

    Regards

    moto

  • FAQ: [#6259] ad73322 channel attribution problem(2010)

    [#6259] ad73322 channel attribution problem

    Submitted By: Bob Liu

    Open Date

    2010-09-17 02:16:18    

    Priority:

    Medium     Assignee:

    Bob Liu

    Status:

    Open     Fixed In Release:

    N/A

    Found In Release:

    N/A     Release:

    Category:

    N/A     Board:

    STAMP

    Processor…

  • [#4230] AD73322 module is not properly installed

    [#4230] AD73322 module is not properly installed

    Submitted By: Vivi Li

    Open Date

    2008-07-10 02:16:44     Close Date

    2008-07-18 08:09:48

    Priority:

    Medium     Assignee:

    Cliff Cai

    Status:

    Closed     Fixed In Release:

    N/A

    Found In Release:

    N/A     Release…