AD7327 can be interfaced with 8Bit SPI Microcontroller Port?
Hi
1. I wanted to know the max supply current for +-15V supply input for AD7327
2. If I don't use a power sequencer for the chip and use the recommended BAT34 schottky diodes only, would it work?
Hi,
I made some study for AD7321 for a while and I thought this chip could meet our requirement. But when I tried to purchase the evaluation board to perform a further evaluation, the system said that EVAL-AD7321 was not recommended for new designs and…
Please give me more information about the AD7327 temperature indicator.
- What is the purpose? Are there the application examples?
- The datasheet describes only Figures 46/47 for specifications. Is there other information? Conversion equation…
I will use the ADC AD7327 (8 channel, Software-selectable input range)
The ADC is powered with +-15V and the signal input range should be set to +-10V.What happens if the input signal voltage is outside the set measuring range?So between +10V to +15V or…
我单独在AD转换芯片加稳定直流电压,转换结果正常。但是将模拟输入端接入经传感器过来的模拟信号时,AD7327转换后的数字量一直为0FFF,我用示波器看了输入电压没有超量程(正负10v)。这是什么原因呢???求指教!!!
AD7327驱动程序
Hello,
We can see some ADC errors on the page 4 in the datasheet of AD7327. Do the specs include an impact of Reference output voltage error (+/-10mV)? Or should we independently count the effect of the Reference output voltage error as those specs for…
I have a question about Figure 46 in the AD7327 datasheet , Rev B . Our application also uses +/10V range, but our Vcc is 3.3V, not 5V as in said figure. How does the curve/equation change for Vcc = 3.3V? Somehow, our software team is using this equation…
AD7327驱动程序 by Viola