• AD7322 Reliability Data

    Hi,

    I'm trying to find the reliability data for the AD7322, e.g. FIT, MTF, etc., and I can't seem to find it. If anyone could help, that would be much appreciated!

    Thanks!

  • RE: AD7322 + SPI

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD7322: Accuracy and precision problem

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Request the Schematic Review with AD7322

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD7322 vs. AD7324 output data range / resolution

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD7322 (or any similar ADC) VHDL model

    Hi,

    Is there a VHDL model for the AD7322 to similar model ADC available that I can use in my testbench? I can modify the code to work for AD7322 if anyone has a similar model. Any help is greatly appreciated.

    Thanks!

  • EVAL-CONTROL BRD2Z Operation

    I am looking at the AD7322 ADC for a precision measurement application. I would not mind having the evaluation board and control features for initial testing, but was wondering if it was a good setup. I see from the datasheets for the controller board…

  • RE: Need help to find out 3.3V, 12-bit, bipolar input (+/-10V range) ADC

    HI Kiran,

    Sorry for the delay in my reply.

    In relation to the ADC. The AD7321 is a relatively new ADC so should be available for the 10 year life time that you have mentioned above. In terms of a second source the AD7322 is pin compatible and functionally…

  • RE: I'm having a problem with the ADA4899 Disable function.

    Charly,

    I'm using a couple more of the the ADA4899 to buffer the input to an AD7322 A/D where I'm letting the DISABLE signal float.  The BW appeals to me and reduced # of different components on the PCB.

    So you think a 499 ohm in the feedback…