• AD7292 End of Live Notice

    We have designed our new product with this AD7292 device for PA biasing and monitoring since the beginning of 2021.

    But we have noticed the message "Not Recommended for New Design" in Analog website for this device recently.

    This may requires…

  • ad7292 spi CPOL is what?

    we need to know the CPOL level of ad7292, but puzzled by the datasheet of EN rev.A and Chinese edition rev.0, due to them don't identity. 

      ....... this is cited from EN rev.A, and there have two dash line pulses of SCLK in CS in disactive state, what mean…

  • AD7292 DAC DISABLE FUNCTION

    How to use the AD7292 Pin 23 or Pin 25 DAC DISABLE to turn on or off the DAC channel output?

    I mean what is the logic level(HIGH or Low) or any voltage level to be applied on the Pin 23 or Pin 25 to turn on/off DAC channel output?

    The data sheet doesn…

  • RE: Alert function in AD7292

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • AD7292驱动程序

    我正在调试.AD7292.但是一直无法读取到ADC数据.和设置DAC.因为这颗AD7292的资源太少.所以希望有大神能够提供帮助.现在强烈的怀疑SPI通讯时序有问题..但是又找不出...有没有人有参考程序....跪求...

    本人使用的是STM32F103系列单片机...

    最好能提供驱动程序.....重谢.!!!

  • RE: Equivalent to AD7292 with 2 alert pin

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • EVAL-AD7292SDZ J5 pinout

    Hi,

    I'm using the EVAL-AD7292SDZ board to test a Linux driver. AD7292 has a GPIO6/BUSY pin which the eval board redirects to connector J5-7. However, I found no information about the numbering of the pins on the J5 connector. Could anyone provide me…

  • RE: ADC used for single-pulse conversion

    Hi Postino,

    Here are some list of ADC that could be suitable for your application. You may also wanted to check the ADI website and do a parametric search and put in parameters on the ADC that you wanted to search. Please refer to the link below.

  • TAGS LIST: Data Converters

    AD693
    AD5410
    AD5412
    AD5420
    AD5422
    AD5735
    AD5755
    AD5755-1
    AD5737
    AD5757
    AD5421
    AD421
    AD5758
    AD7569
    AD7669
    AD7868
    AD7869
    AD5593R
    AD5592R
    AD5940
    AD5941
    AD7293
    AD7294-2
    AD7292
    AD5590
    AD7294
    L…