• AD7266 driver circuit

    Hi

    I have inherited a design in which an AD7266BCPZ is driven by an AD8629 op-amp.

    the AD8629ARNZ uses a chopper architecture, and is bot suitable , to my understanding, for unbuffered SAR driving.

    some oscillation were measured on the amp output (it…

  • Is the AD7266 sensitive to SEU (Single Event Upset)?

    Is the AD7266 sensitive to SEU (Single Event Upset)?

     

    We do not test for SEU type events during the AD7266's qualification phase.
    Therefore, I don’t believe we can provide you with a firm statement on the
    AD7266 sensitivity to SEU. The…

  • AD7266: Timing for analog input selection to CS falling

    What is the min time from Analog input selection ( A0-A2) to CS falling Edge. I
    can't find this information in the datasheet ! And I have some problems when I
    do analog input scanning 1- 6. SCLK speed 24.5MHZ AVDD = VDD = 5V external VREF

  • AD7266: noise (glitch) appears on the input signal

    Hello,

    We have a noise problem on the signals input of the AD7266 converter on a prototype card. During each conversion (conversion frequency = 100 KSPS) a glitch appears on the input signal (see the oscilloscope screenshot).

    But the conversion is correct…

  • AD7266 Clk freq with Vdd=3.3V

    ,Hello

    , I'm using AD7266, Vdd=3.3V, Vdrive=3.3V

    ? I need to sample at list 4 channels in 2us,  so can I use a clock greater than 24MHz

  • RE: AD7266

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD7266

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: BF506F AD7266

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: AD7266 Erratic Readings

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,