• AD7193 Temp measurement in unipolar mode.

    I am using a channel on the AD7193 in unipolar mode. I want to add a temp measurement to the channel sequencer (i.e. enable the channel sequencer and add the temp channel).

    When I do this, I get very strange data, especially given the equation in the…

  • AD7193读取内部温度总是数据异常的大

    AD7193的驱动是从官网上下载下来的,修改的是SPI的接口,无论是单次转换还是连续转换读取温度时,数值总是2000多,第一次使用这个。初始化读ID可以通过。请大神帮忙分析一下。

  • AD7193 Data Rate

    Hello,

    My name is Florian and I'm working for a drone engineering company.

    I just made a PCB by using the AD7193 ADC with a straints gauge to measure the thrust of a dron, and an ATmega328p to convert the SPI data from the ADC to I2C for an other…

  • ad7193 linux驱动读取ID错误

    工程师,我在linux上调试ad7193,总是显示读取ID错误,

    ad7192 spi0.0: device ID query failed (0x3)

    我自己添加代码打印,发现读取的ID一直是0xA3。

    我在该行打印的前面添加读取其它寄存器的打印,发现与datasheet都不吻合。

    ad_sd_read_reg(&st->sd, AD7192_REG_STAT, 1, &id);          //读到 STAT=0x81

    ad_sd_read_reg(&st->sd, AD7192_REG_MODE…

  • AD7193 Supply Voltage & Reference

    SCHEMATIC1 _ PAGE1.pdf

    Hello,

    Please find attached figure.

    I have used REFIN2 by setting REFSEL=1.

    As shown in fig. 3.3V supply is connected to AVDD & REFIN1 is tied to AVDD. Fig. shows Inductor L is connected in series. Instead of L if I Connect Resistor…

  • RE: LabVIEW source code for EVAL-AD7193

    Hello Jellenie R

    Would i be able to get the Labview example code for the AD7193 ?

    Cant see any attachment here...

    thanks

    Jamie

  • Interrupt driven SPI for AD7193

    hello,

    I have started with Soft Implemented SPI for AD7193  & its working fine.

    But now i have added communication facility which is interrupt base.

    Since the ADC is not interrupt driven some samples get corrupted because of high priority interrupt…

  • RE: AD7193 Accuracy Issues...

    Hello mam,

    With respect to above post now i am facing another issue...

    I want to measure this 13mV differential signal proportional to velocity....

    When i apply input from simulator i get stable result but now i am going to test it with actual velocity…

  • RE: AD7193 Differential channel reading zero

    Hi Alex,

    Just got to the verification of the issue today. All the channel works now!!!!!. I changes the Differential channel macros as mentioned above.Thank for your help.

    -SK

  • ad7193 device tree with raspberry pi confiuration

    Hey Guys,

    So i have established communication with ad7193 using raspberry pi and device tree.This is my device tree parting fragment and options available in the ad7193

    So I'm not sure how or where to configure or change gain in the options available…