FAQ
The AD7193 is 4 channel sigma-delta ADC, which is handy for sensor measurement applications - particularly sensors that generate a very small voltage that needs to be measured. Examples include thermocouples and bridge-type sensors (such as load cells). This…
Hello.
The load current is measured by the shunt resistor using AD7193. We observed an AD value of 0xffffff under no load at the site. After that, when a load current of 10A is passed through the returned device, an AD value of about 8A is observed. The…
Hi ,I am using MCU and ADC to build a datalogger for a seismometer.I choose Arduino Mega2560 for MCU and Pmod AD5 for ADC.I have found examples made by Annem (github.com/.../AD7193) and I can read voltage data.
The problem now is that the seismometer sensor…
Hi,
Apologies for missing this query. I am moving this thread to the Precision ADCs community, someone here will be able to assist you on the questions about the AD7193+Arduino Tutorial - Thermocouple Measurements document.
Regards,
Karen
Hi,
Apologies, I would re-direct you the community shown below.
EngineerZone (ez.analog.com) offers support for English language inquiries only. Please post your question in English so that all members can read it. If you require assistance in Chinese…
Hi.
Although conversion is started and data is read periodically, it is safe to put the offset and zero-scale register of AD7193 once a minute for safety by putting them in between. ?
thank you.
Hello everyone,
Can I change the CPOL and CPHA of the AD7193?
Thanks.