• AD7193 + Arduino Tutorial - Thermocouple measurements

    The AD7193 is 4 channel sigma-delta ADC, which is handy for sensor measurement applications - particularly sensors that generate a very small voltage that needs to be measured.  Examples include thermocouples and bridge-type sensors (such as load cells).  This…

  • CN0287 limitations due to common SPI lines (AD5201 & AD7193)

    How to communicate with AD5201 on CN0287 ?
    - Enable and pull down P3 output on AD7193 is done
    - Send data via SPI to AD5201 (SPI bus shared with AD7193)
    - next step should be: Release or pull up P3 output on AD7193, but it is
    possible without error…

  • AD7193 NO LOAD 0xFFFFFF

    Hello.

    The load current is measured by the shunt resistor using AD7193. We observed an AD value of 0xffffff under no load at the site. After that, when a load current of 10A is passed through the returned device, an AD value of about 8A is observed. The…

  • Multiple AD7193 connection and programming suggestion

    Hi ,I am using MCU and ADC to build a datalogger for a seismometer.I choose Arduino Mega2560 for MCU and Pmod AD5 for ADC.I have found examples made by Annem (github.com/.../AD7193) and I can read voltage data.

    The problem now is that the seismometer sensor…

  • RE: AD7193

    Hi,

    Apologies for missing this query. I am moving this thread to the Precision ADCs community, someone here will be able to assist you on the questions about the  AD7193+Arduino Tutorial - Thermocouple Measurements document.

    Regards,

    Karen

  • RE: AD7193采样电压范围

    Hi,

    Apologies, I would re-direct you the community shown below.  

    EngineerZone (ez.analog.com) offers support for English language inquiries only. Please post your question in English so that all members can read it. If you require assistance in Chinese…

  • RE: AD7193数据读取

    你好,我也碰到你这个同样的问题,请问程序中你是怎么解决的?

  • AD7193 offset and zero-scale register.

    Hi.

    Although conversion is started and data is read periodically, it is safe to put the offset and zero-scale register of AD7193 once a minute for safety by putting them in between. ?

    thank you.

  • AD7193 CPOL CPHA

    Hello everyone,

    Can I change the CPOL and CPHA of the AD7193?

    Thanks.